Technical FAQs

Ask a Question

What is the watt rating on the XVE integral steady LED illuminated unit.

Since the consumption ratings of all the LED`s for 240VAC/DC, 24VAC/DC and 120VAC less than 25ma, the wattage ratings are less than 6W, .6W and 3W , respectively.

CTA-ID : 2046216
Was this helpful?
What can we do to improve the information ?