Technical FAQs

Ask a Question

What is the catalog number for the replacement ``PF`` option which is the ``ready to close`` switch on an NW40 ``Drawout`` breaker?

S48469 is the part number for the ``PF`` option ``ready to close`` switch for the NW40 ``Drawout`` type breaker.

CTA-ID : 2046214
Was this helpful?
What can we do to improve the information ?