Technical FAQs

Ask a Question

Are replacement joint bolts available for I-Line (225-600A) amp busway?

No. If the joint bolts are missing, there is a high probability that other parts are missing or misaligned as well. If the outer head has be twisted off, the joint bolt simply needs to be tightened to 70 ft-lbs (+/- 10 ft-lbs) with a proper torque wrench in order to reuse the busway length.

CTA-ID : 2046164
Was this helpful?
What can we do to improve the information ?