Technical FAQs

Ask a Question

What are the repair parts for a HOM816M150FTRB, Series S02, load center?

Only the parts listed below are considered field replaceable:
Cover - 4056317550 (Includes hinges attached to left side of cover)
Cover Mounting Screw - 2142217101 (2 required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure)
Interior Trim with Labels - 4056313301K
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - HOM816M150FTRBI
Neutral Bonding Screw - 4028345850K
Main Breaker - QOM2150VH
Note: Covers and Interior Trims do not have labels applied.

CTA-ID : 2044473
Was this helpful?
What can we do to improve the information ?