Technical FAQs

Ask a Question

Can a 24Vdc, 32A Integral Starter be converted to a 24Vac application?

Yes. The LA1LC080BD DC converter module must be removed and discarded. The LX1D0249 coil must be replaced with a LX1LC020 for 60hz or LX1LC024 for 50hz. Other ac voltages can be obtained by choosing the appropriate coil.

CTA-ID : 2043761
Was this helpful?
What can we do to improve the information ?