Technical FAQs

Ask a Question

What are the repair parts for a HOM1632U200TC, Series S01, load center?

Only the parts listed below are considered field replaceable:
Cover - HOMC20UC
Cover Mounting Screw - 4020513002K
Cover Door Hinge - 4028356450K
Door Latch Kit 4020284450K
Interior Assembly - HOM1632U200TCI
Neutral Bonding Screw - 4028345850K
Equipment Ground Bar - PK18GTA and LK100AN
Main Lugs Kit/Main Breaker - This load center is a Universal Main device which has no Main Lug or Breaker installed. Field install QOL225 for main lug. Field install  QOM2100VH (100 amp), QOM2125VH (125 amp), QOM2150VH (150 amp), QOM2175VH (175 amp) or QOM2200VH (200 amp) for main breaker.

CTA-ID : 2044332
Was this helpful?
What can we do to improve the information ?