Technical FAQs

Ask a Question

What are the repair parts for a QMB363T32W, Series E1 (E01)?<br />

The QMB device is a twin switch, meaning it contains two switches in the one device. One is 100A, the other is 60A. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Complete Arc Suppression Assembly - 3 part numbers required:
(1) Arc suppressor Assembly (1 required) - 4052021450
(1) Arc Shield (top cover) (1 required) - 4052017302
(2) Push nuts (2 required) - 2330241601
Load Base Assembly 100A (1 required, includes lugs) - 4052021650
Load Base Assembly 60A (1 required, includes lugs) - 4052020650
Load Base Mounting Screw (2 required per load base) - 4020506501
Handle Knob Kit - 4028343750
Lug Assembly 100A (per lug) - 4025101851
Lug Assembly 60A (per lug) - 4025101652
Lug Mounting Nut 100A (per lug) - 2342702001
Lug Mounting Nut 60A (per lug) - 2342501700


CTA-ID : 2044331
Was this helpful?
What can we do to improve the information ?