Technical FAQs

Ask a Question

What are the repair parts for a H323NDS Series E1 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40512-570-50 (arc suppressor NOT included)
Load base assembly - 40512-572-50
Arc suppressor assembly - 40520-484-50
Lug assembly - CL10F (includes 6 lugs)
Neutral assembly - H100SNC
Neutral bonding screw - 40283-456-51 (Obsolete - replaced by 40283-656-50)
Cross bar insulator - 40512-318-01
Dust shield - 40512-349-02 (OBSOLETE - NO LONGER AVAILABLE)
Line and load base mounting screws - 40205-065-01
Handle knob kit - 4028344050K ( Series E Switches only)


CTA-ID : 2044243
Was this helpful?
What can we do to improve the information ?