Technical FAQs

Ask a Question

What are the repair parts for a PAK10C1, Series E01, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054005101
Cover Mounting Screws - 2142717161 (2 req`d)
Interior Trim - 4054021101
Interior Trim Mounting Screw - 4020513001K (2 req`d)
Interior Assembly - 4054026150 (Includes the Base Assy, Circuit Breaker(s) and Receptacle(s) listed below. Also includes the neutral assembly, not listed separately)
Base Assembly - 4054025950
Circuit Breaker - QO120GFI
Receptacle - 4054001450
Receptacle Mounting Screw - 2190312160 (1 req`d)
Neutral Bonding Screw - 4028318561
Ground Bar - 4023089990
Ground Bar Mounting Screw - 2159414200 (1 req`d)
Closing Cap - BCAP
Closing Cap Mounting Screw - 2142720241 (1 req`d)
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 2044603
Was this helpful?
What can we do to improve the information ?