Technical FAQs

Ask a Question

Does the catalog numbers CUM400CB, QUM400CL or QUM400CK meet EUSERC specifications?

Product Design Features

Product Line:
Combination Service Entrance Devices

EUSERC Approved

Utility requirements

These CSED Meter-Main devices do not specifically meet EUSERC specifications. However, some EUSERC member utilities may allow them to be used. The utility company should be contacted for their approval before purchasing or installing these devices.

CTA-ID : 2044519
Was this helpful?
What can we do to improve the information ?