Technical FAQs

Ask a Question

on one of the PCF2536, is there a 1400 amp trip unit?<br />

the lowest amp rating that can be achieved is 1600a using the PC31600RC rating column.


CTA-ID : 2044326
Was this helpful?
What can we do to improve the information ?