Technical FAQs

Ask a Question

Can a JDL, JGL, JJL or JLL circuit breaker and GFM250JD ground fault unit be installed into a J250DS enclosure?<br />

This option is not available. Consider using in an I-Line panelboard application.


CTA-ID : 2043703
Was this helpful?
What can we do to improve the information ?