Technical FAQs

Ask a Question

Can an R Frame breaker provide a Ground Fault notification without actually opening the breaker?<br />

If one is installed in the R Frame breaker, a 5.0P trip unit can be used to program the available dry contacts to change state on Ground Fault without tripping the breaker.

CTA-ID : 2044502
Was this helpful?
What can we do to improve the information ?