Technical FAQs

Ask a Question

Which terminal shields are used on the NS400/630N/H/L cable connected to bus bar connected circuit breakers?<br /><br />

Use the ``long pair`` of terminal shields or covers for cable or busbar connected breakers. Note: terminal shields or covers come as standard with UL489 rated breakers, but not on the IEC rated breakers.

CTA-ID : 2044341
Was this helpful?
What can we do to improve the information ?