Technical FAQs

Ask a Question

What are the repair parts for a H323DS Series E2 Heavy Duty Safety Switch?

Repair Parts

Product Line:
Heavy Duty Safety Switches


The parts listed here are the only field replaceable parts.
Line base assembly - 40512-558-50 (arc suppressor NOT included)
Load base assembly - 40512-572-50
Arc suppressor assembly - 40520-214-50
Lug assembly - CL10F (includes 6 lugs)
Cross bar insulator - 40512-318-01
Dust shield - 40512-349-02 (OBSOLETE - NO LONGER AVAILABLE)
Line and load base mounting screws - 40205-065-01
Handle knob kit - 4028344050K ( Series E Switches only)

CTA-ID : 2044242
Was this helpful?
What can we do to improve the information ?