Technical FAQs

Ask a Question

8903LXG40 Can you add power poles?

No, the power pole adders only fit onto an existing 6 pole or 8 pole device. Replace the contactor with the 6 or 8 pole contactor.


CTA-ID : 2043502
Was this helpful?
What can we do to improve the information ?