Technical FAQs

Ask a Question

What are the electrical characteristics of the external power supply module used on the Micrologic A, P and H trip units?

Power supply modules are available in six input voltages:
24/30 Vdc, 48/60 Vdc, 125 Vdc, 110/130 Vac, 200/240 Vac, and 380/415 Vac (all +10%, -15%).
The output voltage for each is 24 Vdc; the output power is 5 VA/5 W (ripple < 5%).


CTA-ID : 2043757
Was this helpful?
What can we do to improve the information ?