Technical FAQs

Ask a Question

Which type of DIN rail is used with the S29305 mounting kit?

It requires 15 mm depth on a 35 mm DIN rail: AM1ED200 for pre-punched and AM1DE200 for no mounting holes.

CTA-ID : 2043426
Was this helpful?
What can we do to improve the information ?