Technical FAQs

Ask a Question

What are the repair parts for an EZML113200, Series M01 branch unit?

Only the parts listed below are considered field replaceable:

Customer Cover (includes labels) - EZML113200C
Cover Screws - 4020513002K
Meter Socket Cover (cover for one meter position) - EZMCRC
Parts Kit (one position, meter socket line side through tenant breaker base) - EZML1200KIT
Circuit Breaker RB Cover (one position) - BCV
Enclosure connecting hardware and Service Disconnect labels - 7329791750
Mounting Channel - 7329771501
Equipment Ground Bar Assembly
Ground Bar Assy. - 7329897052
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP



CTA-ID : 2044059
Was this helpful?
What can we do to improve the information ?