Technical FAQs

Ask a Question

What are the repair parts for a HOM30L200TCK, Series S01, load center?<br /><br />

Only the parts listed below are considered field replaceable.
Cover - HOMC30UC
Cover Mounting Screw - 4020513002K
Door Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit 4020284450K
Interior Assembly - HOM30L200CI
Main Lugs Kit - QOL225
Neutral Bonding Screw - 4028345850K
WireGator Insert - 4055615301 (Includes 1)
WireGator Shields Kit - 4055943550 (Includes 2 shields, mounting screws and 4 slot closures)


CTA-ID : 2043922
Was this helpful?
What can we do to improve the information ?