Technical FAQs

Ask a Question

What is the Terminal Lug Data for a 82355, Series A01, double throw safety switch?

The lugs on this device will accept (1) 1/0 - 600 kcmil aluminum or copper - OR - (2) 1/0 - 300 kcmil aluminum or copper.


CTA-ID : 2043545
Was this helpful?
What can we do to improve the information ?