Technical FAQs

Ask a Question

Is an equipment ground lug supplied with a HU361DS, Series F06, Heavy Duty Safety Switch?

Issue:
Product Features

Product Line:
HD SS

Cause:
Product Features

Resolution:
Yes, two equipment ground lugs are provided factory installed. Each lug will accomodate (1) #14 - 2 aluminum or copper - OR - (2) #14 - 10 aluminum or copper equipment ground conductors.


CTA-ID : 2043531
Was this helpful?
What can we do to improve the information ?