Technical FAQs

Ask a Question

Can 9036GG2R be converted in the field to 9036GG2?

Yes, see the Instruction Bulletin on the adjustments paragraph where it says the bearing pin - A - contacts open; B - contacts close.


CTA-ID : 2043624
Was this helpful?
What can we do to improve the information ?