Technical FAQs

Ask a Question

What is the torque requirements for the joint bolts of a 5000A I-Line II busway?

The required torque value on the joint bolt of all I-Line and I-Line II busway is 70 lb-ft, +/- 10 lb-ft.

CTA-ID : 2043532
Was this helpful?
What can we do to improve the information ?