Technical FAQs

Ask a Question

THIS IS A REVISION TO RESOLUTION # 14563. Revied paragraph number to current #.<br /><br />Is the warranty for a SDSA3650 Surge Arrester valid for applications other than residential?

The only warranty effective for the SDSA3650 Surge Arrester is Paragraph 12 of ``SQUARE D CONDITIONS OF SALE``. This standard warranty is not restricted to residential applications.

CTA-ID : 2043616
Was this helpful?
What can we do to improve the information ?