Technical FAQs

Ask a Question

<br />What contacts can be used in the XALK enclosures?

The ZENL1111 or ZENL1121 contacts will need to be used because they mount in the base of the enclosure. You can use ZB5 operators with the ZENL contacts in the XALD and XALK enclosures.

CTA-ID : 2043611
Was this helpful?
What can we do to improve the information ?