Technical FAQs

Ask a Question

What is the number for the optional lug for one 750 kcmil per phase for the LC, LI, LE, LX,LXI breaker?

It is the AL600LI7. The wire range is for one 500-750 kcmil per phase. Note that catalog number AL600LI7 is for one lug.


CTA-ID : 2043602
Was this helpful?
What can we do to improve the information ?