Technical FAQs

Ask a Question

Can a HDL, HGL, HJL or HLL circuit breaker and GFM150HD ground fault unit be installed into a J250AWK enclosure?<br />

This option is not available. Consider using in an I-Line panelboard application.

CTA-ID : 2043708
Was this helpful?
What can we do to improve the information ?