Technical FAQs

Ask a Question

What is the SCCR (AIC) rating on a 30amp disconnect switch, catalog number 9422TCF30?

Product Line:
9422 type T Disconnect Switches

Resolution: 
The 9422 T Series Disconnect Switch Assemblies are UL Recognized Components. These Switch assemblies when mounted in a correctly sized enclosure and per UL requirements are suitable for use on a circuit capable of delivering not more than 10,000 rms symmetrical amperes at 600 V maximum when protected by Class H or Class K fuses or a maximum of 100,000 rms symmetrical amperes at 600 V maximum when protected by Class J,
or Class R fuses.


CTA-ID : 2043696
Was this helpful?
What can we do to improve the information ?