Technical FAQs

Ask a Question

Does a 9007C54CS17L3 limit switch include a lever arm?

No, purchase the lever arm separately. The 9007C54CS17L3 is configured with an S9 hub for a larger diameter lever arm from the T and FT line. L3 is a corrosion resistant coating.


CTA-ID : 2043688
Was this helpful?
What can we do to improve the information ?