Technical FAQs

Ask a Question

Is a sub feed lug kit available for a CSED catalog number SC1624M125S?

On this CSED, an HOM2125 could be used on the buss as an subfeed breaker, or a HOML2125 sub feed lug kit could also be used. Either option would require 2 spaces on the branch circuit distribution section and can only be used in the top two branch breaker positions.

CTA-ID : 2043596
Was this helpful?
What can we do to improve the information ?