Technical FAQs

Ask a Question

What orientation position should the nameplates be when used with the 9001KR12U1H1?<br />

You can use either vertical or horizontal nameplate orientation. It is shown on page 19-82 of Digest 174; the mechanical interlock will allow spacing to be a minimum of 1 3/4 inches to 2 1/2 inches between the buttons.

CTA-ID : 2043625
Was this helpful?
What can we do to improve the information ?