Technical FAQs

Ask a Question

Can MP Meter-Pak or EZ Meter-Pak Meter Centers be obtained with aluminum enclosures?

Issue:
Are MP and EZM products available in aluminum?

Product Line:
MP and EZM

Environment:
All MP and EZM products

Cause:
Request for aluminum enclosure.

Resolution:
MP and EZM are not available in aluminum enclosures.
As standard our enclosures are constructed of cleaned galvannealed steel, painted with baked on ANSI-49 gray powder coated enamel.


CTA-ID : 2043686
Was this helpful?
What can we do to improve the information ?