Technical FAQs

Ask a Question

Can an old style EZM device be identified by the end closing plate?

Issue:
Application

Product Line:
EZM

Environment:
Old Style ID

Cause:
Identifiying old style vs new style

Resolution:
Yes, the old style end closing plate is approximately 6.5``W x 9.5``H. The new style end closing plate is approximately 5``W x 17``H


CTA-ID : 2043881
Was this helpful?
What can we do to improve the information ?