Technical FAQs

Ask a Question

Are the Class 8502 and 8536 Type S contactors and starters suitable for use on 400 Hertz applications?

No they are not. IEC contactors do have ratings for use on 400Hz.


CTA-ID : 2043832
Was this helpful?
What can we do to improve the information ?