Technical FAQs

Ask a Question

Are the line side bus connectors on an I-Line MA36800 breaker replaceable?

Product Line:

I-Line panelboards and switchboards

Cause:

Care should be taken to determine if the circuit breaker jaws were damaged due to an overheating condition. If this is the case then it is likely the bus bars of the interior are also damaged and should also be inspected.

Resolution:

No, the line side jaws on the breaker are not replaceable. The breaker needs to be replaced.

If the bus bars on the interior are also damaged then the interior should also be replaced as the bus bars are not field replaceable.


CTA-ID : 2043467
Was this helpful?
What can we do to improve the information ?