Technical FAQs

Ask a Question

What is the terminal lug data or main wire size for the CQO48M60DSGP generator panel?

Issue:
Product Design Features

Product Line:
Canadian QO load centers

Environment:
Terminal lug data

Cause:
Installation

Resolution:
The terminal lug data or main wire size for this panel is (1)  #8 - 2 AWG AL/Cu wire.


 
Was this helpful?
What can we do to improve the information ?