Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DT600NKD Neutral Kit?

Product Feature

Product Line:
Safety Switch

Clarifying lug wire range

This neutral provides six terminals, each capable of terminating (1) 250-500 KCMIL AL/CU. There is also a service ground lug capable of terminating (1) #6 AWG - 250 KCMIL AL/CU

CTA-ID : 2043991
Was this helpful?
What can we do to improve the information ?