Technical FAQs

Ask a Question

What are the DC ratings of the MA and MH breakers? There are discrepancies between the Class 601 catalog and Digest 174.

According to the UL procedure the 250 V dc ratings are as follows:

MA, MAL, MAF, MAP are rated 14 kA at 250 V dc
MH, MHL, MHF, MHP are rated 50 kA at 250 V dc


CTA-ID : 2044118
Was this helpful?
What can we do to improve the information ?