Technical FAQs

Ask a Question

What is the interrupting rating of the PXF362000G breaker?

65kA at 600Vac, 100kA at 480Vac, and 125kA at 240Vac


CTA-ID : 2043461
Was this helpful?
What can we do to improve the information ?