Technical FAQs

Ask a Question

What is used to ground the SDA26, auxiliary gutter?

There is a Ground Lug or Terminals - Catalog # - QOGL20, and there should be a grounding lug or Terminal in each SDAG26 auxiliary gutter to maintain the ground through each SDAG26, auxiliary gutter .




CTA-ID : 2044886
Was this helpful?
What can we do to improve the information ?