Technical FAQs

Ask a Question

Is there a sensor that meets NEMA 7 & 9, explosion proof, Class 1, Division 1, Hazardous Locations?<br />

We do not offer an explosion proof sensor that meets NEMA 7 & 9 for gases (Class1). We do offer sensors for hazardous dusts (Class 2) built to the ATEX D standard. These require a separate amplifier to operate (NY3 series.)

CTA-ID : 2044852
Was this helpful?
What can we do to improve the information ?