Technical FAQs

Ask a Question

Does an XS2M30MA230K come with a cable?<br /><br />

No, It has a AC/DC micro style quick disconnect connector and no cable. The suffix K or U20 codes indicate this type of connector. Example: cable would be the XSZCK101Y (1.8 Meter) with 90 degree molded connector.




CTA-ID : 2044850
Was this helpful?
What can we do to improve the information ?