Technical FAQs

Ask a Question

What is a NEMA M-1P Manual Starter?

That is a 2 pole 5hp 230v Starter. NEMA standards only allow for one designation other than a number for sizing starters and that is the 1P designation to allow for a 5Hp/230v single phase motor. In this case the M prefix means Manual starter.


CTA-ID : 2044673
Was this helpful?
What can we do to improve the information ?