Technical FAQs

Ask a Question

What are the repair parts for a PAK54C, Series E01, ServicePak Power Outlet Panel?<br />

Only the parts listed below are considered field replaceable.
Cover - 4054005101
Cover Mounting Screws - 2142717161
Interior Trim - 4054021401
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4054023750 (Includes the Base Assy, Circuit Breaker(s) and Receptacle(s) listed below)
Base Assembly - 4054023950
Circuit Breaker - QO250
Receptacle - 4054004050
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 2044635
Was this helpful?
What can we do to improve the information ?