Technical FAQs

Ask a Question

What are the part numbers to install an NQOD30L225 or NQOD430L225 interior in an MH44 box?<br /><br /><br />

The following parts will be required per panel:

(2) 80110-288-04 (12`` rail extensions)
(1) 80110-291-04 (12`` MLO deadfront extension)
(2) 80110-289-01 (deadfront mounting brackets)
(4) 21590-17081 (rail extension screws)
(2) 80025-067-01 (deadfront screws)

These parts replace the main breaker kit.




CTA-ID : 2044387
Was this helpful?
What can we do to improve the information ?