Technical FAQs

Ask a Question

What are the optional lugs for a QMB363TW and QMB363HW, Series E1, and what wire sizes do these lugs accommodate?

40251-018-50 - AL/CU Mechanical lugs that accept #12 to 1/0
40256-014-50 - CU mechanical lugs that accept #14 to 1/0
VCEL02114S1 - AL crimp lugs that accept #8 to 1/0
VCELC02114S1 - CU crimp lugs that accept #6 to 1/0


CTA-ID : 2044818
Was this helpful?
What can we do to improve the information ?