Technical FAQs

Ask a Question

Is the S29390 24VDC Shunt trip accessory and 29390 24VDC shunt trip accessory the same?

Both are 24VDC shunt trip accessories, but the S29390 is a UL lised, field installable shunt trip, for the Powerpact H and J frame breakers. The 29390 is also a 24VDC shunt trip accessory , but for the Compact IEC version , NSJ and NSF breakers. They are functionally the same , but are marked are marked differently, one UL (S29390) vs IEC (29390)


CTA-ID : 2044813
Was this helpful?
What can we do to improve the information ?