Technical FAQs

Ask a Question

Are the operating mechanism for the GS1 Switches replaceable?

The operating mechanism that is part of the switch base itself is not a replaceable part. A new switch will have to be purchased. The handle and shaft can be replaced separately.


CTA-ID : 2044827
Was this helpful?
What can we do to improve the information ?