Technical FAQs

Ask a Question

Can a FAL32080 be applied on a 400hz system, 240v?

It is not UL listed for application at 400Hz, but may be so applied if UL is not required. Must rerate the breaker`s magnetic performance and interrupting rating per bulletin 0100DB0101 available from the intranet.

CTA-ID : 2044795
Was this helpful?
What can we do to improve the information ?